990-9137889A-001

Configure the Display Preferences

  1. Tap Configuration > General > Display.
    1. Set the Alarm sound to Enable or Disable. This will enable/mute all alarm sounds.
    2. Set the Alarm sound (informational alarms only) to Enable or Disable. This will enable/mute all informational alarm sounds.
    3. Set the temperature unit to Celsius or Fahrenheit.
    4. Set the Screen saver on after to 5 min, 15 min, 30 min, or Never. The screen saver will turn on after the set time where no activity has been performed on the display.
    5. Set the Display brightness by tapping the - or +.
    6. Set the Touch screen sound to Enable or Disable. This will enable/mute all display sounds (excluding alarm sounds).
    7. Calibrate the touch functionality of the display by tapping the calibration button twice.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.