990-9137889A-001

Overview of User Interface

Display

Overview of the Home Screen

  1. Home button - tap this button on any screen to return to the home screen.

  2. Main menu button - tap this button on any screen to access the menus.

  3. Mimic diagram button - tap this button on any screen to access the mimic diagram.

  4. Alarm status symbol - tap this button on any screen to access the active alarms log.

You can tap on the output or battery fields on the home screen to go directly to the detailed measurement pages.

Mimic Diagram

The mimic diagram will adapt to your system configuration – the mimic diagrams shown here are just examples.

Example of Single UPS System – Dual Mains

The green power line (gray in illustration) in the mimic diagram shows the power flow through the UPS system. Active modules (inverter, rectifier, battery, static bypass switch, etc.) are framed in green and inactive modules are framed in black. Modules framed in red are inoperable or in an alarm condition.

NOTE: The mimic diagram only shows one battery disconnect device BB even if more battery disconnect devices have been connected and configured for monitoring. If one or more of the monitored battery disconnect devices are in the closed position, the BB on the mimic diagram will show as closed. If all of the monitored battery disconnect devices are in the open position, the BB on the mimic diagram will show as open.

In mimic diagrams for parallel systems, tap on the gray UPS to see the mimic diagram on UPS level.

Example of Parallel System – Dual Mains with Individual UIB and SSIB

Alarm Status Symbol

The alarm status symbol (gray in illustration) in the top right corner of the display changes depending on the alarm status of the UPS system.

Green: No alarms present in the UPS system.
Blue: Informational alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Yellow: Warning alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.
Red: Critical alarm(s) present in the UPS system. Tap the alarm status symbol to open the active alarms log.

Menu Tree

  • Status

    • Input

    • Output

    • Bypass

    • Battery

    • Temperature

    • Power modules

    • Peak shaving

    • Parallel*

  • Logs

  • Control*

    • Operation mode

    • Inverter

    • Charger

    • Guided sequences

  • Configuration*

    • UPS

    • Output

    • Battery

      • Standard

        • General settings

      • Custom

        • General settings

        • Specific settings

    • High efficiency

      • Schedule

    • Grid interactive UPS

      • Protected Modbus

    • Breakers

    • Contacts and relays

    • Network

    • Modbus

    • General

    • Reminder

    • Save/restore

    • Update status

  • Maintenance

    • Buzzer

    • Status LEDs

    • Breaker lamp

    • Battery*

    • Runtime calibration*

    • Battery replacement*

    • Battery SPoT mode*

    • UPS report*

  • Statistics

  • About

  • Logout

  • Flag button – Tap this button to set the display language.

Some menus contain more submenus than described in this manual. These submenus are grayed out and are only for use by Schneider Electric to avoid unwanted load impacts. Other menu items can also be grayed out/not shown on the display if they are not relevant or not released yet for this particular UPS system.

System Level Controller (SLC) and Unit Controller (UC) Overview

  1. Inverter ON/OFF buttons

  2. USB ports*

  3. Universal I/O*

  4. Modbus port*

  5. USB Micro-B port*

  6. Network port*

  7. Reset button*

  8. Status LEDs*

  9. Display power supply

  10. Display port

  11. Service port*

  12. EXT port

  13. For future use

  14. PBUS 1*

  15. PBUS 2*

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.