990-91460A-001

Installation Procedure for Easy UPS 3L with Bottom Entry Cabinet

NOTE: All power cables and signal cables can be routed through the bottom entry cabinet and connected in the UPS.
  1. Install the Bottom Entry Cabinet with the Easy UPS 3L.
  2. Follow the UPS installation manual to connect the power cables and the signal cables and to complete the rest of the UPS installation.
QR code for this page

Was this helpful?