990-91460A-001

Install the Seismic Anchoring with the Galaxy VL UPS (Option)

Use the optional seismic kit GVLOPT002 for this procedure.

  1. Connect the rear anchoring assemblies for the UPS and the bottom entry cabinet with the interconnection plate.

    Rear View

  2. Mount the rear anchoring assembly to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchors is ø16 mm. The minimum requirement is M12 strength grade 8.8 hardware.

    Rear View

  3. Remove all the screws and the interconnection plate.

    Rear View

  4. Remove the anchoring brackets.

    Rear View

  5. Install the rear anchoring brackets on the UPS and the bottom entry cabinet with the provided M8x25 bolts.

    Rear View of the UPS and the Bottom Entry Cabinet

QR code for this page

Was this helpful?