Resetting day counter

The meter is equipped with a day counter for consumed energy. The consumed energy can be reset to zero (0).
To reset the day counter to zero (0), follow these steps:
  1. Scroll to LCD resettable kWh (KWh 0) page in the main menu.
  2. Hold the button for 3 seconds to enter the menu.
  3. When the value starts blinking: hold the button for 5 seconds to reset the day counter (KWh 0).
  4. The LCD displays OK when the day counter (KWh 0) is reset.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?