Setting up Scrolling time

  1. Scroll with the button to Program mode 2 (PM0dE2).
  2. Hold the button for 3 seconds to enter the menu.
  3. Scroll to LCD cycle time (RT xx) page.
  4. Hold the button for 5 seconds to enter program mode.
  5. When the value starts blinking: select the new value between 1 – 30 seconds.
  6. Hold the button for 3 seconds to confirm the new scrolling time.
  7. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?