Setting up parity

The Modbus parity can be set to even, none or odd.
To change the parity, follow these steps:
  1. Scroll with the button to Program mode 3 (PM0dE3).
  2. Hold the button for 3 seconds to enter the menu.
  3. Enter the 4 digit password: scroll with the button and select each digit 0 – 9, hold the button for 3 seconds to confirm each digit. Default password is 0000.
  4. Scroll to LCD parity (PArity xxxx) page.
  5. Hold the button for 5 seconds to enter program mode.
  6. When the value starts blinking: select even/none/odd.
  7. Hold the button for 3 seconds to confirm the new setting.
  8. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?