DOCA0145EN-00

Firmware Update with EcoStruxure Power Commission Software

EcoStruxure Power Commission is the new name of Ecoreach software.

Use the latest version of EcoStruxure Power Commission software to:

  • Check the firmware compatibility of the devices in the IMU

  • Update the devices with the latest firmware version available

After updating the firmware of one device, use EcoStruxure Power Commission software to check the firmware compatibility between IMU devices.

The Firmware Update table helps the user to diagnose and identify all discrepancy issues between IMU devices. This table also provides the recommended actions for each discrepancy issue.

The latest version of EcoStruxure Power Commission software is available at www.se.com.

For more information on the use of EcoStruxure Power Commission software, refer to EcoStruxure Power Commission Online Help.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.