DOCA0145EN-00

IFM Modbus-SL Interface for One Circuit Breaker

The IFM Modbus-SL interface for one circuit breaker (IFM interface) enables an intelligent modular unit (IMU) containing a circuit breaker equipped with a communicating MicroLogic trip unit to be connected to a two-wire Modbus-SL RS-485 serial line Modbus network.

Each circuit breaker has its own IFM interface and a corresponding Modbus address.

The IFM interface with part number TRV00210 or STRV00210 is compatible with the following ranges of circuit breaker:

  • MasterPact NT/NW circuit breakers

  • ComPact NS circuit breakers

  • ComPact NSX circuit breakers

  • PowerPact P- and R-frame circuit breakers

  • PowerPact H-, J-, and L- frame circuit breakers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.