DOCA0145EN-00

Firmware Version 002.002.016

New Features

  • Integrated the retry mechanism for optimizing the data continuity of service (automatic bus resynchronisation and automatic disconnection with device as it is silent for more than one minute).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.