Certifications and Standards

Agency Certifications

  • Underwriters Laboratories Inc., UL 61010-2-201 and CSA C22.2 N°61010-2-201, for Industrial Control Equipment used in Ordinary Location

  • Underwriters Laboratories Inc., UL 121201 and CSA C22.2 N°213, for Industrial Control Equipment used in Class I, Division 2 Hazardous (Classified) Locations

  • IECEx / ATEX for use in zone 2 gas /zone 22 dust

Compliance Standards

Europe:

CE

  • Directive 2014/30/EU (EMC)

Australia:

  • RCM

Korea:

  • KC

Hazardous Substances

  • RoHS, Directive 2011/65/EU and 2015/863/EU

  • RoHS China, Standard GB/T 26572

  • REACH regulation EC 1907/2006

End of Life (WEEE)

KC Markings

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.