Commissioning
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Verify the following:
- The equipment is correctly installed. Check the level adjustment and floor anchoring.
-
All high and low voltage electrical connections have been correctly installed and tested. If any of the three-position isolating switch with ground functions are not going to be in operation and are without incoming cables, the corresponding grounding switch must be closed and locked by means of a padlock to avoid possible misoperation. It is advisable to fit insulating caps on the connectors, which provide identical electrical and mechanical characteristics as the “T” connectors. These insulating caps can be ordered from the connector supplier.
-
Mechanical operation of all devices (three-position isolating switch with ground, and so forth) and the interlocks of each unit.
It is important to carry out the following operations:
-
Five manual closing/opening operations
-
Five electrical closing/opening operations
-
Five opening operations by tripping coil
-
After performing all the checks described above, perform the high voltage cable tests detailed in Cable Test.
The incoming cables are now ready to be energized, while keeping the corresponding three-position isolating switch with ground in the open position.
Check for the following:
-
Voltage presence on cables. The indications of the voltage presence indicator system must not be used as absence of voltage indicator. Always use a properly rated voltage sensing device to confirm power is off. Refer to Live Line Indicator (LLI).
-
Concordance of phases
Once all requirements are fulfilled, the unit is ready to be put into service by operating the circuit breakers.
DANGER