Transportation, Receiving, Handling, and Storage
This section contains instructions for receiving, handling, and storing DVCAS outdoor switchgears. Follow all safety precautions before working on the equipment.
Transportation
WARNING |
|---|
|
TOP-HEAVY LOAD
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
UNBALANCED LOAD OR EQUIPMENT DISTORTION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Products travel on the client´s own account, unless otherwise requested. Therefore, the company declines any responsibility regarding problems of supply. All products are labeled with the following information to assist carriers with proper handling.
There are two proper methods for transporting the equipment, as shown in the preceding table:
-
Use a fabric lifting strap of sufficient length to have greater than or equal to 45 degrees between the strap and the roof of the equipment.
-
Use fabric lifting straps on the left and right and front and back sides of the unit, maintaining an angle (≥ 45 º).
If using a forklift, refer to the figure below and follow these practices:
-
Secure the equipment to the forklift with a safety strap.
-
Ensure the equipment is bolted to the pallet.
Receiving
The packaging was developed to help protect the switchgear during transportation includes a wooden pallet especially designed for using a lifting crane from its lower side. The packaging has wooden walls and a roof to help protect the switchgear from damage during lifting and transport.
Immediately inspect the equipment for any damage that may have occurred in transit. Once it is inspected, compare the packing list to the equipment received to make sure the order and shipment are complete.
Claims for shortages or errors must be made in writing to Schneider Electric within 60 days of delivery. Failure to give such notice will constitute unqualified acceptance and a waiver of all such claims by the purchaser.
If damage is found or suspected, file a claim with the carrier immediately and notify Schneider Electric. Delivery of the equipment to a carrier at any of the Schneider Electric plants or other shipping point constitutes delivery to the purchaser regardless of freight payment and title. All risk of loss or damage passes to the purchaser at that time.
Follow completely the DVCAS Receiving Check List provided in the next section and in addition:
-
Check that the material included in the spare part box agrees with the provided list of pieces.
-
In case of disagreement, please file a claim to the transport company, stating the order number, damaged material, nature and cause of the damage. To ensure the warranty of the material, fill in the report and notify the technical service center, so that the period of warranty of the material is regularized from the date of delivery.
Receiving Check List
DVCAS Receiving Check List
| Date: | |||||
| Project Name: | |||||
| Serial No.: | |||||
| Location: | |||||
| Certified Schneider FSR: | |||||
| Schneider PM / Sales Leader: | |||||
| This checklist must be completed with photos. Photo mandatory for each “Not OK” response. | |||||
| Description | OK | Not OK | Photo No. | ||
| 1. | No impacts or damage in transport packaging. | ||||
| 2. | No damage or impact on paint surface. | ||||
| 3. | Check that the nameplate of the cubicle matches the project work order. | ||||
| 4. | No loose or missing screws or rivets, no gaps in DVCAS. | ||||
| 5. | Main enclosure cover operates correctly (no misalignment). | ||||
| 6. | Cubicle nameplate matches project work order. | ||||
| 7. | SF6 pressure level on each cubicle is approximately 0.3 bar. | ||||
| 8. | No loose material or wiring in Low Voltage cabinet. | ||||
| 9. | Protection cap properly installed on each cubicle bushing and Voltage Transformer (VT) bushing. | ||||
| 10. | Control Transformers (CTs) and VTs securely fastened and secondary wiring connected. | ||||
| 11. | All steel parts installed to attain required performance (enclosure, IAC). | ||||
| 12. | General appearance of stickers, mimics, and covers is good. | ||||
| 13. | Circuit breaker, three-position isolating switch with ground, interlocks operate properly. See Annex 1. | ||||
| 14. | Phase continuity (phase-to-phase) tested by closing the circuit breaker and three-position isolating switch with ground. Phase continuity (bushing-to-bushing) of each section tested. | ||||
| Comments | |||||
| FSR Signature: | |||||
| PM Signature: | |||||
Handling
WARNING |
|---|
|
tip over hazard
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
Incorrect lifting components
Do not replace any lifting kit components.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
WARNING |
|---|
|
UNBALANCED HEAVY LOAD OR EQUIPMENT DISTORTION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Avoid:
-
Blows and sudden movements which may harm the components
-
Leaving the equipment on non-flat, unstable, or wet surfaces
-
Moving or sliding the equipment along inclined planes or stairs
Although the product offers a high degree of robustness, inside the structure are several mechanisms and insulating parts which require careful handling. It is therefore advisable to use fork-lift trucks or cranes with enough power and capacity for their handling.
The unit can be unloaded and transported by means of a fork-lift truck or a crane. In case of using a crane to elevate the unit, pay attention to the center of gravity and handle the unit in a balanced way.
Lifting Instructions for Installation
Safety Provisions
This section provides instructions for using the Lifting Accessory Kit. Please read and follow the instructions in this manual before performing the instructions in this section and read all instructions in this section before performing any steps contained in it.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
List of Components
WARNING |
|---|
|
Incorrect lifting components
Do not replace any lifting kit components.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Lifting Process Preparation
WARNING |
|---|
|
handling and lifting hazard
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
- Remove the wrapping.
- Unscrew the wooden base from the switchgear.
- Attach fabric lifting straps to a crane hook.
- Remove the bolts from the two anchoring brackets from the left and right hand sides of the unit.
- Flip the anchoring brackets over 180° and install all the bolts. Apply torque of 17-23 ft-lb [23-30 N•m] on M8 bolts.
- Mount the eye bolts on the left and right hand side of the unit. Apply torque of 44-60 ft-lb [60-80 N•m] on 5/8-11 hex nuts.
- Attach fabric lifting strap to four lifting eyes on either side of the unit. Do not use chains or cables.
Lifting and Handling
- Move the switchgear to the mounting surface.
- Detach the fabric lifting straps.
- Remove four eye bolts.
- Remove the bolts from the four anchoring brackets in front and back of the unit.
- Flip the anchoring brackets over 180° to the original position and install all the bolts. Apply torque of 17-23 ft-lb [23-30 N•m] on M8 bolts.
Moisture Contamination Avoidance and Mitigation
DANGER |
|---|
|
hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
|---|
|
Fire Hazard
Remove all flammable material in the vicinity of the heaters,
such as packaging, accessories in boxes, and documentation, before
energizing the heaters.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Shipping, Receiving, and Storage Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be stored in a climate-controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment are not suitable for outdoor storage.
-
Treat the equipment as if it is in storage until it is installed and operational. The storage area must be clean, dry (75% or less relative humidity), and climatecontrolled with proper ventilation.
-
To keep the equipment dry, use of heaters is required in some cases (for example, during seasonal or low periods of electrical loading and equipment deenergization).
-
Consult the engineer of record for the appropriate environmental control settings or means to mitigate environmental influences.
-
If so equipped, set the thermostats and/or humidistats to mitigate condensation. A minimum of 95 W of heat per section is recommended.
-
If heaters are used with the equipment that were not included in the equipment by Schneider Electric, they must be clean and free of debris and grease. Greasy and/or smoky heaters can contaminate electrical insulation and lead to dielectric breakdown and/or tracking.
-
-
Shipping packaging is not suitable for and cannot be used by itself for outdoor equipment storage unless otherwise indicated on the shipping packaging labeling.
-
When receiving equipment, the equipment may be at a lower temperature than the ambient air temperature. Allow time for the equipment temperature, including the temperature of internal components, to rise to the ambient air temperature before making openings in or otherwise disturbing the packaging. Condensation can occur on and inside the equipment if warm air contacts cold surfaces of the equipment. Moisture damage can occur, destroying the dielectric capabilities of the equipment and rendering it unusable.
-
The factory shipping wrap around the equipment on shipping pallets is not suitable for non-enclosed (no tarp) over-the-road transportation that risks exposing the equipment to the elements. Leave the factory shipping wrap around the equipment on the equipment until the equipment is ready for inspection and stored or inspected and installed. After receiving the equipment and allowing it to acclimate to the environment, remove the packaging and inspect the equipment for damage that may have occurred in transit. If damage is found or suspected, immediately file a claim with the carrier and notify your Schneider Electric representative.
-
Follow these guidelines every time the equipment is moved to a new storage location or to its destination.
Installation, Operation, and Maintenance Requirements
This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be operated in a climate-controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment are not suitable for outdoor storage.
In some cases (such as seasonal electrical loading, de-energized equipment, and standby/alternate power sources), the heat generated by equipment loading is insufficient to help prevent condensation and alternate heat sources are required. If environmental controls such as a thermostat or humidistat are used, their settings must be sufficient to mitigate condensation and always remain operational. Consult the engineer of record for the appropriate environmental control settings.
Shock Detectors
WARNING |
|---|
|
equipment distortion
Confirm if any of the shock detectors is activated before
installation.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
Two shock detectors are installed on the equipment, one on the front side and the other on the lateral side. Check them when receiving the equipment. If any detector was activated, contact your Schneider Electric point of contact.
Storage
The equipment is designed for outdoor installations; it is recommended to store it in an indoor environment before the assembly and commissioning operations.
Maximum recommended storage time is three months from delivery.
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Store the switchgear indoors under the following conditions:
Failure to follow these instructions will result in death or serious injury.
|
WARNING
DANGER