JPS7801200

Safety Provisions

Before installing, operating, or maintaining this equipment, read and understand this bulletin, all steps described herein, and all schematics and electrical diagrams.

Electrical equipment should be installed and serviced only by qualified electrical personnel in accordance with national and local electrical codes.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, or NOM-029-STPS-2011.
  • This equipment must only be installed and serviced by qualified, trained, and certified electrical personnel.
  • Only qualified electrical personnel familiar with medium voltage circuits should perform the instructions in this bulletin. Personnel must understand the hazards involved in working with or near medium voltage equipment.
  • Qualified electrical personnel must perform work in accordance with national and local electric codes.
  • Perform such work only after reading and understanding all of the instructions in this bulletin.
  • Before performing assembly, visual inspections, testing, or maintenance on the equipment, disconnect all sources of electric power. Assume that all circuits are live until they have been completely de-energized, tested, grounded, and tagged. Pay particular attention to the design of the power system. Consider all sources of power, including the possibility of back-feeding.
  • Never disconnect the main trip source of energized equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Before making any electrical connections, ensure that all leads to be connected are de-energized and proper safety grounds are applied.
  • Metal enclosed switchgear has interlocks designed to minimize hazards to the user. The user of this device is responsible for recognizing the potential hazards, for wearing personal protective equipment, and for taking adequate safety precautions.
  • Do not make any adjustments to the equipment or operate the system with safety features removed. Contact your local Schneider Electric representative for additional instructions if the device does not function as described in this manual.
  • Handle this equipment carefully and install, operate, and maintain it correctly in order for it to function properly.
  • Ensure that the ground circuit is correctly assembled.
  • Preventive maintenance operations must be carried out regularly.
  • Follow regular inspection, checking the gas pressure and condition of the external elements, and carry out the usual cleaning task. Refer to Maintenance Program.
  • Carefully inspect your work area and remove any tools and objects left inside the equipment.
  • Replace all devices, doors, and covers before turning on the power to this equipment.
  • All instructions in this manual are written with the assumption that the customer has taken these measures before performing installation, operation, maintenance, or testing.
Failure to follow these instructions will result in death or serious injury.
DANGER
INSULATING GAS LEAKAGE
Do not drill into or open the pressurized container.
Failure to follow these instructions will result in death or serious injury.
DANGER
moving parts in mechanical drive
  • See important safety information on page 7.
  • Release the circuit breaker energy storage device by ON-OFF-ON operation of the circuit breaker.
  • Switch the appropriate grounding to the grounded position.
  • Do not remove mechanism during maintenance work.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Do not operate or install any equipment that appears damaged.
Failure to follow these instructions will result in death or serious injury.
WARNING
Potential compromise of system availability, integrity, and confidentiality
  • Change default passwords to minimize instances of unauthorized access to device settings and information.
  • Disable unused ports/services and default accounts, where possible, to minimize pathways for malicious attacks.
  • Place networked devices behind multiple layers of cyber defenses (such as fire walls, network segmentation, and network intrusion detection and protection).
  • Use cyber security best practices (for example, least privilege and separation of duties) to minimize chances of unauthorized exposure, loss, modification of data and logs, interruption of services, or unintended operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
toppling or falling
  • While handling the moving devices, pay attention to uneven floor surfaces (for example, cracks, projections, and so on) in the switchgear room.
  • Consult with a certified lifting and rigging expert for any situation not covered in these instructions.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Damage to the Top Portions of the Equipment
  • Do not walk upon the topsides of the switchgear panels.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
SHARP-EDGED SHEET METAL AND METAL PARTS
During installation and maintenance work:
  • Always wear the approved protective clothing in accordance with the applicable accident prevention and work regulations.
  • Always cover sharp edges.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
DOOR ASSISTED UPWARD WITH STORED ENERGY
  • Follow the information in the equipment drawings, instruction bulletin, and local and national codes and standards for the required clearances around the equipment, especially in the front.
  • Maintain full control of the door during closing or opening operations.
  • Do not stand or place objects within 65 inches of the front door during its opening or closing operations.
  • Ensure door is fully open before releasing control of the door.
  • Ensure the door is secured shut with captive hardware before releasing control of the door.
  • It is mandatory that the door stay referenced in Step 4 of Front Door Cover Operation - Open be positioned as soon as the door is opened.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Personnel must be fully familiar with the instructions and warnings contained in this manual and with general requirements of the legislation in force.

Recycling Your Equipment at End-of-Life

SF6 is a powerful greenhouse gas having a Global Warming Potential of 22800 compared to CO2 (in accordance with the 4th IPCC assessment report and annex I of EU regulation on fluorinated gases 517/2014).

WARNING
RELEASE OF DANGEROUS SUBSTANCES
  • Do not release the SF6 gas into the environment. The SF6 gas must be extracted for recycling or destruction before disposal of the device at the end of its service life.
  • Obtain appropriate approval before performing disassembly work.
  • Only allow certified personnel to handle SF6 gas.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Contact your local Schneider Electric representative for obtaining relevant material related to recycling information regarding the proper disposal of DVCAS series gas insulated switchgear and its components.

Registered Trademarks and Copyright

All names of registered trademarks referred to in this document are the property of their respective owners.

Proposition 65 Notice

Before installing, operating, or maintaining this equipment, read and understand this bulletin, all steps described herein, and all schematics and electrical diagrams.

WARNING: This product can expose you to chemicals including lead and lead compounds, which are known to the State of California to cause cancer and birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?