DOCA0223EN-02

Tool Configuration

Automatic discovery is not available in the firmware upgrade tool. The list of Link150 gateways for which the firmware is to be updated are described and written manually in a user-created .csv file.

Follow the standard rules of .csv file format when editing the configuration file.

An example of the .csv file is shown below:

Each line corresponds to one gateway. The three columns describe the IP address of the gateway, user login account and password.

NOTICE
UNINTENDED ACCESS TO CONFIDENTIAL DATA
  • Once all the devices are updated, encrypt the file and protect it with a password to save the file integrity and confidentiality. Most compression utilities can perform such operation.
  • Store the encrypted archive file in a location on a PC or a network directory where access controls are enforced to help prevent any unauthorized access to the file.
Failure to follow these instructions can result in unauthorized or unintended access to data.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.