6055-30, Rev. 4

Safety Precautions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, or Arc Flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462.
  • This equipment must be installed and serviced only by qualified electrical personnel.
  • Perform such work only after reading and understanding all of the instructions contained in this bulletin.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Before performing visual inspections, tests, or maintenance on this equipment, disconnect all sources of electric power. Assume all circuits are live until they are completely de-energized, tested, and tagged. Pay particular attention to the design of the power system. Consider all sources of power, including the possibility of backfeeding.
  • Always practice lock-out/tag-out procedures according to OSHA requirements.
  • Open all circuit breaker and switch contacts and discharge all springs before performing maintenance work, disconnection, or removal of a circuit breaker.
  • Move circuit breakers to the disconnected position before removing rear access panels.
  • Conduct electrical testing to confirm no short-circuits were created during installation, maintenance, or inspection.
  • Never insert a circuit breaker into a circuit breaker compartment that is not complete and functional.
  • The complete assembly arrangement determines if the top or bottom contacts are the line side; both can be energized when the circuit breaker is removed from the compartment. Identify the line side contacts for each circuit breaker compartment.
  • Disconnect all high voltage to the switchgear before accessing the horizontal bus compartment.
  • Do not use liquid fire extinguishers or water on electrical fires. Before extinguishing fires within the assembly, ensure the main power source is disconnected and the main and all feeder circuit breakers are open.
  • Carefully inspect your work area, and remove any tools and objects left inside the equipment.
  • Replace all devices, doors, and covers before turning on power to this equipment.
  • All instructions in this manual are written with the assumption that the customer has taken these measures before performing maintenance or testing.
Failure to follow these instructions will result in death or serious injury.

WARNING: This product can expose you to chemicals including Nickel compounds, which are known to the State of California to cause cancer, and Bisphenol A (BPA), which is known to the State of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov.

Moisture Contamination Avoidance and Mitigation

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Store the equipment in a clean, dry (including no condensation), well-ventilated area with an ambient temperature of approximately 70°F (21°C).
  • If heaters are furnished in the assembly, energize them from an external source. When energizing heaters from an external source, remove the primary and secondary overcurrent protective devices from the control power transformer.
  • If heaters are not installed in the assembly, and the area is cold and damp, use a temporary heating source within the assembly. A minimum of 200 W of heat per section is recommended.
  • Avoid greasy, smoky heaters that can deposit carbon on insulation, which could lead to tracking and insulation breakdown.
  • If moisture, condensation, or chemical ingress is observed, do not energize the equipment. If the equipment is already energized, de-energize it immediately.
Failure to follow these instructions will result in death or serious injury.
WARNING
Fire Hazard
Remove all flammable material in the vicinity of the heaters, such as packaging, accessories in boxes, and documentation, before energizing the heaters.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Shipping, Receiving, and Storage Requirements

This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be stored in a climate-controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.

  • The equipment should be treated as if it is in storage until it is installed and operational. The storage area should be clean, dry (75% or less relative humidity), and climate controlled with proper ventilation.

  • To keep the equipment dry, the use of heaters is required in some cases (for example, during seasonal or low periods of electrical loading and equipment de-energization):

    • Consult the engineer of record for the appropriate environmental control settings or means to mitigate environmental influences.

    • If so equipped, set the thermostats and/or humidistats to mitigate condensation. A minimum of 200 W of heat per section is recommended.

    • If heaters are used with the equipment that were not included in the equipment by Schneider Electric, they must be clean and free of debris and grease. Greasy and/or smoky heaters can contaminate electrical insulation and lead to dielectric breakdown and/or tracking.

  • Shipping packaging is not suitable for and cannot be used by itself for equipment storage unless otherwise indicated on the shipping packaging labeling.

  • When receiving equipment, the equipment may be at a lower temperature than the ambient air temperature. Allow time for the equipment temperature, including the temperature of internal components, to rise to the ambient air temperature before making openings in or otherwise disturbing the packaging. Condensation can occur on and inside the equipment if warm air contacts cold surfaces of the equipment. Moisture damage can occur, destroying the dielectric capabilities of the equipment and rendering it unusable.

  • The factory shipping wrap around the equipment on shipping pallets is not suitable for non-enclosed over-the-road transportation that risks exposing the equipment to the elements. The factory shipping wrap around the equipment should remain on the equipment until the equipment is ready to be inspected and stored or inspected and installed. After receiving the equipment and allowing it to acclimate to the environment, remove the packaging and inspect the equipment for damage that may have occurred in transit. If damage is found or suspected, immediately file a claim with the carrier and notify your Schneider Electric representative.

  • Follow these guidelines every time the equipment is moved to a new storage location or to its final destination.

Installation, Operation, and Maintenance Requirements

This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be operated in a climate controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.

In some cases (such as seasonal electrical loading, de-energized equipment, and standby/alternate power sources), the heat generated by equipment loading is insufficient to prevent condensation and alternate heat sources are required. If environmental controls such as a thermostat or humidistat are used, ensure their settings are sufficient to mitigate condensation and remain operational at all times. Consult the Engineer of Record for the appropriate environmental control settings.

Exposure to Moisture, Chemicals, and Condensation

If liquids such as moisture, chemicals, and condensation contact the electronics, circuit breaker, fuses, bussing, or other electrical components, do not attempt to clean or repair the equipment as this may lead to unrepairable damage. If the equipment is energized, de-energize it. If equipment is not energized, do not energize it. Contact the Schneider Electric Customer Care Center at 888-778-2733.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.