6055-30, Rev. 4

Installation

Site Preparation

DANGER
HAZARD OF electric shock, explosion, or arc flash
  • Install the equipment in a clean, dry (including no condensation), well ventilated area with an ambient temperature of approximately 70°F (21°C).
  • Place dust covers over circuit breakers.
  • If heaters are furnished in the assembly, energize them from an external source. When energizing heaters from an external source, remove the primary current limiting fuses from the control power transformer.
  • If heaters are not installed in the assembly and the area is cold and damp, use a temporary heating source within the assembly. A minimum of 200 W of heat per section is recommended.
  • Avoid greasy, smoky heaters that can deposit carbon on insulation that could lead to tracking and insulation breakdown.
Failure to follow these instructions will result in death or serious injury.
WARNING
Fire Hazard
Remove all flammable material in the vicinity of the heaters, such as packaging, accessories in boxes, and documentation, before energizing the heaters.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

This equipment does not achieve its ratings until it is installed per record/as-built drawings, installed per the instructions contained in this document, and has operational environmental controls with appropriate settings to help mitigate environmental influences. This equipment can also be operated in a climate controlled area that uses both heating and cooling to maintain acceptable environmental conditions. Indoor and outdoor rated equipment is not suitable for outdoor storage.

In some cases (such as seasonal electrical loading, de-energized equipment, and standby/alternate power sources), the heat generated by equipment loading is insufficient to prevent condensation and alternate heat sources are required. If environmental controls such as a thermostat or humidistat are used, ensure their settings are sufficient to mitigate condensation and remain operational at all times. Consult the engineer of record for the appropriate environmental control settings.

Good site preparation is essential for operation of the assembly. Carefully compare the plans and specifications with the customer drawings provided. Be sure to:

  • Provide adequate ventilation at all times so the ambient temperature around the assembly does not exceed 104°F (40°C). Supply clean, dry, filtered air.

  • Provide adequate lighting in both the front and back aisle spaces. Also provide convenience outlets in both areas for electrical hand tool use.

  • Provide adequate floor drains

  • Route sewer, water, and steam lines so they do not pass over or near the assembly. Dripping liquids that enter the equipment will cause damage.

  • Do not allow water to collect or run under the equipment

  • Do not install the equipment over locations that could retain moisture, such as a cable vault, without sealing the equipment to not allow moisture to enter the equipment.

Exposure to Moisture and Chemicals

If liquids such as moisture, chemicals, and condensation contact the electronics, circuit breaker, fuses, bussing, or other electrical components, do not attempt to clean or repair the equipment as this may lead to unrepairable damage. If the equipment is energized, de-energize it. If equipment is not energized, do not energize it. Contact the Schneider Electric Customer Care Center at 888-778-2733.

Weights

The weight of the average complete switchgear unit is 2500–2900 lb. (1134–1315 kg) for up to 50 kA and 3200 lb. (1451 kg) for 63 kA. Refer to Switchgear and Component Weights and Individual Components to determine switchgear and component weights for handling and structural considerations.

Switchgear and Component Weights

Item Rating Weight

Switchgear unit*

Up to 50 kA

2100 lb. (952 kg)

63 kA

2400 lb. (1089 kg)

Circuit breaker

1200 A, 25 kA

380 lb. (172 kg)

1200 A, 40 kA

380 lb. (172 kg)

1200 A, 50 kA

430 lb. (195 kg)

2000 A, 25 kA

430 lb. (195 kg)

2000 A, 40 kA

450 lb. (204 kg)

2000 A, 50 kA

500 lb. (227 kg)

3000 A, 50 kA

700 lb. (318 kg)

1200, 2000, and 3000 A, 63 kA

800 lb. (363 kg)

4000 A, 50 kA

700 lb. (318 kg)

4000 A, 63 kA

800 lb. (363 kg)

Up to 50 kA, 15 kV

210 lb. (95 kg)

63 kA, 15 kV

273 lb. (124 kg)

Up to 50 kA, 15 kVA

270 lb. (122 kg)

Drawout VT unit (two VTs)

63 kA, 15 kVA

333 lb. (151 kg)

Drawout CPT unit

37.5 kVA

580 lb. (263 kg)

CPT fixed mounted

50 kVA

750 lb. (340 kg)

Surge arresters (three intermediate)

15 kV

120 lb. (54 kg)

Individual Components

Item

50 kA

63 kA

Total Fan Assy

229 lb. (104 kg)

229 lb. (104 kg)

Base

164 lb. (74 kg)

168 lb. (76 kg)

Foundation

The switchgear is designed for installation on a concrete pad. Refer to the factory order drawings for any additional mounting details which may be required on specific orders. The pad must be flat and leveled to 0.06 in. (1.6 mm) per square yard to help ensure proper alignment and to help prevent distortion of the gear.

Provide a seven ft. (2.1 m) wide aisle space in front of the mounting pad, flush with and finished to the same tolerance as the mounting pad. This level surface is necessary for the circuit breaker lift truck and for inserting the circuit breakers into the bottom compartment.

Floor Plan for Switchgear Rated Up to 50 kA

Masterclad Extended Floor Plan for 63 kA-Rated Switchgear

NOTE: A minimum of three ft. (1 m) is necessary on the right end facing the front of the line-up. This space is necessary for door clearance, with door hinges on the right side of the door, when removing the circuit breakers. Typically, a minimum of three ft. (1 m) is necessary at the rear of the lineup for cable connections.

Stub conduits a maximum of one inch. (25 mm) above floor level. To simplify moving the switchgear into place, keep the conduit flush with the surface of the floor. Position the conduit accurately so that there is no mechanical interference with the assembly frame. Eliminate continuous loops of reinforcing rod or structural steel that do not enclose all conductors of the same circuit. Floor Plan for Switchgear Rated Up to 50 kA and Masterclad Extended Floor Plan for 63 kA-Rated Switchgear illustrate typical floor plans. Refer to the customer order drawings before using the typical foundation specifications. Customer order drawings are created to comply with specific customer requirements and therefore supersede the information provided here.

Switchgear Installation

Pre-Installation Procedures

  1. The switchgear may be shipped in one or more shipping sections. Review the assembly drawings to verify that switchgear sections will be assembled in the correct order.

  2. Verify that the conduit placement on the foundation is accurate according to customer drawings. Error in conduit placement may prohibit the proper installation of switchgear as described in this section (see the note below).

  3. Sweep the pad and remove debris before installing any sections.

Installation

NOTE: When more than two shipping sections are involved, any error in conduit location can cause a cumulative error significant enough to prohibit the proper installation by the assembly sequence described in this section. To lessen cumulative error, unload and install the center shipping section first and work toward either end.
  1. Move the sections, with skids attached, into place. Install the shipping section that allows the most maneuverability first. If rollers must be used, move with the skid in place. Remove the skid only when the switchgear is in proper position on the pad. Lower the first section onto the pad. Do not pry directly on the structure, doors, or covers.

  2. Before proceeding, verify:

    • The conduits are in the center of the cutouts.

    • The back of the unit is perpendicular to the pad and has proper clearance.

    • The mounting holes line up with the mounting channels.

  3. Move an adjacent switchgear shipping section into place.

  4. Level each section before installing the next. Install steel shims, when necessary, between floor channels and switchgear.

  5. Verify that the switchgear sections are level, aligned, and fit snugly together. If the sections do not fit properly, lift the most recently placed section by crane, remove any obstructions, and re-install.

  6. Bolt switchgear shipping sections together.

    NOTE: All shipping sections must be bolted together in place before bolting them to the channel sills or installing the horizontal main bus.
  7. Repeat steps 4–5 for additional switchgear shipping sections.
  8. Verify that all switchgear shipping sections are in the correct position according to the job drawing after all sections are bolted together.
  9. Install all cable compartment floor plates to create a barrier between cable compartment and space below the switchgear.

3000 A sections with auxiliaries on the top have the two rear bolt locations covered by a ventilation duct. In order to access those two locations, the two screws holding the ventilation boxes on left and right side need to be removed. Then the entire ventilation duct can be slid forward to access the anchor points. Replace the duct to its original position once the switchgear is bolted or welded.

Access to Rear Bolt Locations in Auxiliary-3000 A Sections

Main Bus Installation

Install the main bus at the shipping split only after all sections are securely anchored in place and no additional movement of the assembly occurs. Bus bar extensions for shipping splits are shipped with the miscellaneous items.

A typical main bus assembly is shown in (see Main Bus Assembly). The side and rear views (see Main Bus Assembly) of the assembly show the general arrangement of the main bus and riser. The side (see Main Bus Connections-Side View) and top (see Main Bus Connections-Top View) views show the different bus connections and the orientation of the filler and splice plates. When aluminum bus is furnished, some of the circuit breaker connections and splice or filler plates are copper.

Main Bus Assembly

Main Bus Connections-Side View

Main Bus Connections-Top View

The standard switchgear is furnished with fiberglass-polyester bus barriers between bays. Porcelain “pass-throughs” are available as an option for 50 kA and below only.

Main Bus Pass-Through, Porcelain—Optional for 50 kA and Below Only

For porcelain pass-throughs only, O-rings must be installed inside the passthroughs to cushion the bus bars under short-circuit conditions.

Schneider Electric recommends the following installation steps for installing two bus bars:

  1. Place the larger O-ring around both bars at the correct distance from the end, and the smaller rings around each bar approximately one inch (25 mm) on each side from the large O-ring.

  2. Slide both bars into the porcelain (one end of the porcelain may have a larger opening).

    NOTE: When bus bar stand-off insulator installation is required on shipping sections, fiberglass/polyester washers and rubber O-rings must be installed as shown.

    Stand-Off Bus Support

  3. Remove the main bus covers and the insulating boots.

  4. Install one phase at a time by sliding the bus bar through the bus barriers and loosely bolting the horizontal bus to the vertical bus. Do not bend or force the bus to make this connection. The through bushings and the divided insulating barrier may be loosened if necessary. They have sufficient clearance and adjustment to compensate for minor field misalignment of shipping sections.

  5. Tighten the bolts holding the bus bar joints only after all three bus bars are in place and properly fitted. Use a torque wrench to make sure that the bolts for bus bar connections are tightened in accordance with recommended bolt torque values.

  6. Reinstall all boots ensuring they are properly closed.

Bolt Torque Values

Bolt Size

Mechanical Joints

Bus bar Connections

1/4–20

4–7 lb-ft. (5.4–9.5 N•m)

5/16–18

11–15 lb-ft. (14.9–20.3 N•m)

3/8–16

18–24 lb-ft. (24.4–32.5 N•m)

30–40 lb-ft. (40.7–54.2 N•m)

1/2–13

32–44 lb-ft. (43.4–59.7 N•m)

47–62 lb-ft. (63.7–84.0 N•m)

Ground Bus Connection

DANGER
hazard of electric shock, explosion, or arc flash
Connect the ground bus to the proper equipment ground per the local installation code requirements. The ground bus must be connected for proper operation of relaying and instrumentation, and for personnel safety.
Failure to follow these instructions will result in death or serious injury.

Control Wiring Connections

Consult the customer wiring diagram for reconnection of wiring at the shipping break. Each wire is identified and has been previously connected during assembly and verified at the factory. If the identification is missing or blurred, ring-out before connecting to avoid control circuit and instrument panel problems at start-up.

Initial Circuit Breaker Installation

Follow these instructions for the initial install of the circuit breaker:

  1. De-energize all primary and control power circuits.

  2. Insert each circuit breaker into the connected position of its respective circuit breaker compartment. Observe the operation of the ground contacts, shutters, and disconnect position latch.

  3. Remove each circuit breaker from its compartment. Open the shutters and check that tracks made in the contact grease by the fingers of the main disconnects extend back a minimum of 0.5 inch (13 mm) from the front edge of each bar. Make sure that the ground shoe leaves tracks on the ground bus.

Do not force circuit breakers into circuit breaker compartments. Compartment rating interlocks help prevent inserting circuit breakers into incorrect sections.

VT, CPT, and Fuse Drawout Installation

  1. Withdraw the drawout control power fuse drawer and the drawout voltage transformer drawer. Observe their operation. Verify that the static grounding contacts touch the moving drawout contacts and that the primary and secondary contacts make proper contact.

  2. Prior to energization, verify spacing of all VT, CPT and fuse drawout cabling.

    The VT Cables are designed to run parallel and perpendicular to the barriers across their length in the cubicle. They are positioned and spaced correctly (from phase and ground) by the porcelain.

  3. Verify the cables are routed properly and the porcelain bushings are not displaced from their designed location. Visually inspect for any damage to the insulation or accumulation of dust on the cable on both sides of the barrier.

    Examples of Cable Breakers

  4. If there is any visible sign of damage, replace the cables. Clean possible dust accumulation with a lint free cloth and denatured alcohol. Two types of cable pass through insulators are used within Masterclad, a porcelain bushing and a nylon cable gland. The cable gland was introduced to the assemblies in 2021. If the equipment contains nylon cable glands to route cables, disregard the information pertaining to porcelain bushings.
  5. Make sure that all the VT cables pass freely through the porcelain bushings without stressing their placement in the barrier.

  6. The bushings cannot tilt or displace because of interference with the cables. If needed, reshape the cables so that their axes match the axes of the bushing bores.

  7. Make sure the O-rings are firmly in place in their mounting grooves.

O-rings and Mounting Grooves

In general, the cables must always maintain the following minimum clearances:

 

Voltage ≤ 5 kV in. (mm)

5 kV ≤ Voltage ≤ 15 kV

Phase to Phase

3 (76.2)

4 (101.6)

Grounded Metal

3 (76.2)

4 (101.6)

For additional information on proper field installation of customer cabled transformer connections, refer to document 46010-520.

High-Potential Testing

Before making external power connections, perform a high-potential (hi-pot) dielectric withstand test on the bus and circuit breakers as an assembly.

Use a reliable transformer-type tester with a built-in voltmeter and milliamp meter for hi-pot testing. Capacitor loaded bench-type testers with neon bulb indicators do not have sufficient capacity to give reliable results.

Test Preparation

  1. Disconnect surge arresters.

  2. Withdraw the voltage transformer drawer (if provided).

  3. Place each of the circuit breakers in its proper circuit breaker compartment in the connected position. Charge their springs manually, and then close each circuit breaker by using the CLOSE (I) push button.

Phase-to-Phase Test

  1. Perform a phase-to-phase hi-pot test on the main bus:

    1. Gradually increase the voltage to the levels shown in Table 5.

    2. Verify that the equipment sustains the specified voltage without flashover for one minute.

  2. Turn off the test equipment. Discharge the phase bus to ground before removing the test cables.

Phase-to-Ground Test

  1. Perform a phase-to-ground hi-pot test on the main bus:

    1. Gradually increase the voltage to the levels shown in List of Supported Regional Building Codes and Seismic Design Standards.

    2. Verify that the equipment sustains the specified voltage without flashover for one minute.

  2. Turn off the test equipment. Discharge the phase bus to ground before removing the test cables.

Refer to List of Supported Regional Building Codes and Seismic Design Standards for the nominal test values for dry, clean, new assemblies. Field hi-pot tests are made at 75% of factory test voltages in accordance with ANSI standards.

One Minute Hi-Potential Test*

Assembly Rated Maximum Voltage

Factory Test Voltage (AC)

Field Test Voltage

AC

DC

5 kV

19 kV

14 kV

20 kV

15 kV

36 kV

27 kV

38 kV

If satisfactory results are not obtained, locate the problem, correct it, and rerun the test before proceeding. If the issue seems to be occurring in the vacuum interrupter, change the polarity and rerun the test. If this resolves the issue, the vacuum interrupter is fit for duty. If results are acceptable, the power cables, ground wires, external wiring, and battery (if supplied) can be connected to the assembly. If results are not acceptable, contact your local Schneider Electric representative.

Phasing

In accordance with NEMA standards, all bus within the switchgear is phased A-B-C left to right, top to bottom, and front to back when viewing the assembly from the front (the circuit breaker compartment side). If, for any reason, the bus must be phased differently, the different phases are identified on the bus with a label.

Equipment Anchorage for Non-Seismic Applications

The equipment enclosure provides anchorage tie-down points to accept anchor attachments to the building structure or foundation. Masterclad 5-15 kV Metal-Clad indoor enclosures provide enclosure base frame clearance holes to accept bolted anchorage attachments as shown in Non-seismic Switchgear Anchor Assembly. Four anchors are required for each section, two in the front and two in the rear located per the Floor Plan for Switchgear Rated Up to 50 kA and Masterclad Extended Floor Plan for 63 kA-Rated Switchgear.

Non-seismic Switchgear Anchor Assembly

Equipment Installation for Seismic Applications

Introduction Seismic Certification

Seismic certification is an optional feature on the Masterclad 5-15 kV Metal-Clad product line and provides seismic conformance options to any of the North American and International building codes and seismic design standards identified in Table 5. Masterclad 5-15 kV Metal-Clad that is seismically certified has been certified to the seismic requirements of the listed code per the manufacturer’s certificate of compliance (CoC). Equipment compliance labels and CoC’s are provided with all seismically certified Masterclad 5-15kV Metal-Clad. Refer to the equipment CoC for certification details and applicable seismic parameters. To maintain the validity of this certification, the installation instructions provided in this section must be followed.

List of Supported Regional Building Codes and Seismic Design Standards

Country / Region

Code Reference ID

Code Name

North American Codes

Canada

NBCC

National Building Code of Canada

Mexico

CFE MDOC-15

Civil Works Design Manual, Earthquake Design

United States

IBC per ASCE 7
CBC per ASCE 7
UFC per DoD

International Building Code—IBC
California Building Code—CBC
Uniform Facilities Criteria—UFC

International Codes

Argentina

INPRES-CIRSOC103

Argentinean Standards for Earthquake Resistant Constructions

Australia

AS 1170.4-2007 (R2018)

Structural design actions, Part 4: Earthquake actions in Australia

Chile

NCh 433.Of1996

Earthquake resistant design of buildings

China

GB 50011-2010 (2016)

Code for Seismic Design of Buildings

Colombia

NSR-10 Título A

Colombian Regulation of Earthquake Resistant Construction

Europe

Eurocode 8 EN1998-1

Design of structures for earthquake resistance – Part 1: General rules, seismic actions and rules for buildings

India

IS 1893 (Part 1) : 2016

Criteria for Earthquake Resistant Design of Structures Part 1 General Provisions and Buildings

Indonesia

SNI 1726:2019

Earthquake Resistance Planning Procedures for Building and Non-building Structures

Japan

Building Standard Law

The Building Standard Law of Japan

New Zealand

NZS 1170.5:2004+A1

Structural design actions, Part 5: Earthquake actions – New Zealand

Peru

N.T.E. - E.030

National Building Code, Earthquake-Resistant Design

Russia

СП 14.13330.2018

Building norms and regulations: Construction in seismic regions

Saudi Arabia

SBC 301

Saudi Building Code, Loads & Forces Requirements

Taiwan

CPA 2011

Seismic Design Code and Commentary for Buildings

Turkey

TBEC-2018

Turkey Buildings Earthquake Standard

Responsibility for Mitigation of Seismic Damage

The Masterclad 5-15 kV Metal-Clad equipment is considered a nonstructural building component as defined by regional building codes and seismic design standards. Equipment capacity was determined from tri-axial seismic shake-table test results in accordance with the International Code Counsel Evaluation Service (ICC ES) Acceptance Criteria for Seismic Certification by Shake-Table Testing of Nonstructural Components (ICC-ES AC156).

An equipment importance factor, Ip, that is greater than one (Ip>1.0) is assumed and indicates that equipment functionality is required after a seismic event and after seismic simulation testing. This importance factor is applicable for designated seismic systems (for example, special certification) servicing critical infrastructure and essential buildings where post-earthquake equipment functionality is a requirement.

Incoming and outgoing bus, cable, and conduit must also be considered as related but independent systems. These distribution systems must be designed and restrained to withstand the forces generated by the seismic event without increasing the load transferred to the equipment. For applications where seismic hazard exists, it is preferred that bus, cable, and conduit enter and exit the bottom of the equipment enclosure.

Seismic certification of nonstructural components and equipment by Schneider Electric is just one link in the total chain of responsibility required to maximize the probability that the equipment will be intact and functional after a seismic event.  During a seismic event the equipment must be able to transfer the inertial loads that are created and reacted through the equipment’s force resisting system and anchorage to the load-bearing path of the building structural system or foundation.

Anchorage of equipment (for example, nonstructural supports and attachments) to the primary building structure or foundation is required to validate seismic conformance. The construction site structural engineer or engineer of record (EOR) or the registered design professional (RDP) is responsible for detailing the equipment anchorage requirements for the given installation. The installer and manufacturers of the anchorage system are responsible for assuring that the mounting requirements are met. Schneider Electric is not responsible for the specification and performance of equipment anchorage systems.

Tie-down Points for Rigid Floor Mounted Equipment

The equipment enclosure provides anchorage tie-down points to accept anchor attachments to the building structure or foundation. Masterclad 5-15 kV Metal-Clad indoor enclosures provide enclosure base frame clearance holes for bolted anchorage attachments. Equipment installations must be anchored using all enclosure tie-down points as shown in Floor Plan for Switchgear Rated Up to 50 kA and Masterclad Extended Floor Plan for 63 kA-Rated Switchgear.

Equipment installations using welded supports and attachments in lieu of bolted supports and attachments must ensure the weld locations are distributed similarly to the locations of enclosure anchorage clearance holes. Welded supports and attachments must be properly sized to ensure the weldment withstand capacity exceeds the earthquake demand at location of equipment installation. Precautions shall be made to properly vent and shield the equipment enclosure during the field welding process. Schneider Electric is not responsible for equipment damage caused by field welded supports and attachments.

Anchorage Assembly Instructions

The bolted anchor assembly view depicted in Switchgear as Tested Anchor Assembly illustrates the equipment’s as-tested attachment to the seismic shake-table test fixture. The equipment seismic rated capacity, as stated on the Schneider Electric CoC, was achieved with the identified size and grade attachment hardware. For bolted attachments, the use of factory supplied Belleville conical spring washers, are required to maintain seismic conformance. Field installed equipment attachment and support detailing shall be in accordance with the anchorage system requirements as defined by the construction site EOR or RDP.

Switchgear as Tested Anchor Assembly

Cable Connections

Before making cable connections, install the cable compartment floor plates.

Be very careful when making up all types of cable terminations, as terminations are critical to the successful operation of the electrical distribution system. Avoid sharp turns, edges or corners to help prevent damage to the cable insulation. Follow the cable manufacturer’s recommendations for minimum bending radius. These instructions vary from manufacturer to manufacturer.

Solderless or compression-type cable lugs are the most common method for connecting power cables to metal-clad switchgear. When making the terminations for each type of power cable, follow the cable manufacturer’s instructions. After the cable connections are made, insulate them with the boots if provided, or as follows:

  1. Place 3M™ Scotchfil™ electrical insulating putty around the lugs and bolts to reduce the concentrated field created by their irregular shapes (see Non-seismic Switchgear Anchor Assembly). Apply a layer of 3M Scotch® 13 electrical semiconducting tape over the Scotchfil. Half-lap the tape, which must extend onto the conductor. Do not extend the tape up over the bus epoxy insulation. Apply 3M Scotch 130C splicing tape over the Scotch 13 tape. Half-lap this tape for two layers on 4.76 kV installations, and four layers on 8.25 kV and 15 kV installations. For 4.76 kV applications, extend this tape 1.5 inch (38 mm) up over the bus insulation and cable insulation. Extend the tape two inch (51 mm) for 15 kV applications.

  2. Apply two layers of 3M Scotch 22 electrical tape, extending the tape up over the Scotch 130C tape in all directions. The tape and other insulating materials for completing these field connections are not supplied with the switchgear.

  3. When terminators are supplied for terminating power cables, follow the power cable manufacturer’s instructions for terminating the cables in these devices. To facilitate installation of the power cables, the bus side is not taped. After the cables are installed, insulate the terminator-to-bus connections according to the cable lug insulation instructions in this section.

High Voltage Cable Lug Insulation

NOTE: The external surface of each shielded cable is at ground potential and must be positioned a minimum of six inches (152 mm) from any live part (even its own pole), including insulated bus bars.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.