6055-48, Rev. 2

Introduction

This bulletin contains instructions to receive, handle, store, and install Square D Masterclad 27 kV, Outdoor Non-Walk-in, Metal-Clad Switchgear. The non-walk-in enclosure described in this bulletin is bolted onto standard indoor switchgear.

NOTE: This bulletin must be used in conjunction with instruction bulletin 6055-40 Masterclad Metal-Clad Indoor Switchgear, 27 kV with Type VR Vacuum Circuit Breakers.

Outdoor Non-Walk-in Switchgear

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.