BQT8706400-00

Civil Engineering with a Cable Trench

MV Cables Rear Entry

Intended for cables up to 240 mm2.

Not recommended for 630 mm2 cables.

Figure 24
MV Cables Rear Entry

MV Cables Entry from the Side Near a Wall

Intended for cables up to 240 mm2.

Not recommended for 630 mm2 cables.

Figure 25
MV Cables Entry from the Side near a Wall

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?