DOCA0247EN-00

About the Book

Document Scope

The aim of this guide is to provide users, installers, and maintenance personnel with the technical information needed to operate the factory-installed Inverse Definite Minimum Time (IDMT) Ground-fault Digital Module. It includes information about:

  • The Advanced protection menu available on the MicroLogic X display screen to set IDMT ground-fault protection

  • IDMT ground-fault protection

All information concerning the MicroLogic X control unit can be found in DOCA0102EN MasterPact MTZ – MicroLogic X Control Unit – User Guide.

This guide applies to the following MicroLogic X and MicroLogic Xi control units.

Standard

Control units

Commercial reference

IEC

MicroLogic 2.0 X

LV847600

MicroLogic 5.0 X

LV847602

MicroLogic 2.0 Xi

LV857600

MicroLogic 5.0 Xi

LV857602

UL

MicroLogic 3.0 X

LV848815

MicroLogic 5.0 X

LV847609

MicroLogic 3.0 Xi

LV857610

MicroLogic 5.0 Xi

LV857609

NOTE: The commercial reference is printed on the front face of the MicroLogic X and Xi control unit. It also identifies the standard, IEC or UL.
NOTE: A MicroLogic Xi control unit is a MicroLogic X control unit without Bluetooth® Low Energy communication.

All the information related to the MicroLogic X control units presented in this guide applies to MicroLogic Xi control units except information about Bluetooth Low Energy communication.

The specific features of the MicroLogic Xi control units are described in the appendix of DOCA0102EN MasterPact MTZ – MicroLogic X Control Unit – User Guide.

Validity Note

This guide applies to MicroLogic X and Xi control units with firmware version

@updated
005.103.000 or greater, and with IDMT Ground-fault Digital Module factory-installed.

For a MicroLogic X control unit with a lower firmware version, refer to DOCA0144EN MasterPact MTZ - MicroLogic X Control Unit - Firmware Release Notes for a description of the new features and bugs fixed in subsequent firmware versions.

Online Information

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download.

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric home page at www.se.com.

Related Documents

Title of documentation Reference number
MasterPact MTZ – MicroLogic X Control Unit – User Guide DOCA0102EN
MasterPact MTZ - MicroLogic X Control Unit - Firmware Release Notes

DOCA0144EN

MicroLogic Trip Units and Control Units - Firmware History

DOCA0155EN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.