DOCA0247EN-00

Protection Menu

Description

The Protection menu contains the following submenus:

Level 1

Level 2

Level 3

Function description

Home

Protection

I long time

Long-time overcurrent protection, L or ANSI 49RMS/51

I short time(1)

Short-time overcurrent protection, S or ANSI 50TD/51

I instantaneous

Instantaneous overcurrent protection, I or ANSI 50

I neutral

Neutral protection

Dual settings

Dual settings

Advanced

IDMT ground-fault protection

(1) Applies to MicroLogic 5.0 X for IEC and UL standards

Only the Advanced submenu is described in this guide. For the description of other submenus, refer to DOCA0102EN MasterPact MTZ – MicroLogic X Control Unit – User Guide

Active Settings

Active settings used by the protection functions are displayed in the Quick View.

The settings in the Protection menu are the settings defined by the user. They may differ from the settings used by the protection functions when Fallback settings mode is active.

For more information, refer to DOCA0102EN MasterPact MTZ – MicroLogic X Control Unit – User Guide

Advanced

The Advanced menu presents the following data and settings:

Level 3

Level 4

Level 5

Parameter name

Advanced

IDMT GF

Protection

Enable IDMT ground-fault protection function:

  • OFF: the following menus are not displayed and the ground-fault protection is not active.

  • ON: the following menus are displayed.

Action

IDMT ground-fault protection action:

  • Trip

  • Alarm

Inhibit

Enable inhibit by IO module:

  • OFF

  • ON

Curve

I4t, for display only.

Ig (A)

Ig ground-fault protection threshold expressed in Amps.

IgMax (A)

Maximum Ig ground-fault protection threshold expressed in Amps.

tg (s)

tg ground-fault protection time delay.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.