EcoStruxure Power Device App

Presentation

EcoStruxure Power Device app is a single mobile application with the necessary information and capabilities to operate and efficiently maintain devices in the EcoStruxure architecture.

The application enables you to connect to devices, including the following:

  • MasterPacT MTZ circuit breakers

  • TeSys GV4 motor circuit breakers

  • Easergy P3 protection relays

The application can be installed on a smartphone by downloading the application from:

  • Google Play Store for Android smartphones

  • App Store for iOS smartphones

MasterPacT MTZ Devices in EcoStruxure Power Device App

With the EcoStruxure Power Device app, a smartphone can be used with MasterPacT MTZ devices as the primary interface for day-to-day and critical case maintenance. The MicroLogic X control unit is identified on the application by scanning the QR code on the device.

When the EcoStruxure Power Device app is used in conjunction with a Digital Module, additional functions are available:

  • With the Power Restoration Assistant Digital Module, tutorials are available, providing information about restoring power and identifying the causes of trips.

  • With the MasterPacT Operation Assistant Digital Module, remote control of the circuit breaker is available.

Wireless communication is available by Bluetooth and NFC communication. A USB OTG connection is also available.

Using a Bluetooth Low Energy Connection

The MicroLogic X control unit must be powered to establish a Bluetooth Low Energy connection.

Using EcoStruxure Power Device app with a Bluetooth Low Energy connection gives access to and allows sharing of the information types organized in the following tabs:

  • Quick View: gives an overview of current values per phase, the health state of the circuit breaker, and recent event history.

  • Metering: displays values of RMS current, RMS voltages, network, and energy in real time.

  • Protection Setting: displays settings currently selected and allows modification of settings.

  • Maintenance and Diagnostic:

    • Displays maintenance reminder, service life, actuator wear, contact wear, and diagnostic counters.

    • Interprets contact wear to estimate the circuit breaker ability to isolate, withstand rated duty, operate, and trip.

  • Status and Control:

    • Displays status of the circuit breaker.

    • Allows opening and closing operations to be carried out when the MasterPacT Operation Assistant Digital Module is installed.

When Digital Modules are installed on the MicroLogic X control unit, additional information is available.

For more information, refer to the Bluetooth Low Energy connection procedure.

Using a USB OTG (On-The-Go) Connection

The MicroLogic X control unit can be powered by a smartphone using the USB OTG connection, if necessary.

Using EcoStruxure Power Device app with a USB OTG connection gives access to and allows sharing of the following information types organized in the following tabs:

  • Quick View: gives an overview of current values per phase, the health state of the circuit breaker, and recent event history.

  • Metering: displays values of current, RMS voltages, network, and energy in real time.

  • Protection Setting: displays settings currently selected and allows modification of settings.

  • Maintenance and Diagnostic:

    • Displays maintenance reminder, service life, actuator wear, contact wear, and diagnostic counters.

    • Interprets contact wear to estimate the circuit breaker ability to isolate, withstand rated duty, operate, and trip.

  • Status and Control:

    • Displays status of the circuit breaker.

    • Allows opening and closing operations to be carried out when the MasterPacT Operation Assistant Digital Module is installed.

When Digital Modules are installed on the MicroLogic X control unit, additional information is available.

For more information, refer to the USB OTG (On-The-Go) connection procedure.

Using an NFC Connection

Connecting to EcoStruxure Power Device app with an NFC connection is always possible, even when the MicroLogic X control unit is not powered. It gives access to the following information:

  • Information about the MicroLogic X control unit

  • Last trip context: trip type; date and time of last trip; current values before trip

  • Protection settings (display only)

  • Access to Power Restoration Assistant or MasterPacT Operation Assistant Digital Modules

For more information, refer to the NFC connection procedure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?