DOCA0102EN-12

Bluetooth Low Energy Communication

Description

A Bluetooth LED

B Bluetooth activation button

C Serial number of MicroLogic X control unit

Using Bluetooth Low Energy communications, you can access the MicroLogic X control unit from a smartphone running the EcoStruxure Power Device app. This application offers a task-oriented interface with the control unit.

You can establish a Bluetooth Low Energy connection with only one MicroLogic X control unit at the same time. Only one smartphone at a time can connect to a control unit.

During the connection, the control unit is identified by the last digits of its serial number. The format of the identifier is MTZ <ProtectionType> <EndOfSerialNumber>, for example, MTZ 5 012345, where 5 indicates MicroLogic 5.0 X control unit and 012345 are the last 6 digits of the serial number.

Bluetooth Low Energy communications are encrypted using Advanced Encryption Standard (AES) 128-bit encryption.

Prerequisites for Using Bluetooth Low Energy Connection

The prerequisites for establishing a Bluetooth Low Energy connection are:

  • The MicroLogic X control unit must be powered.

  • Bluetooth Low Energy communication must be enabled on the control unit.

  • You must have a smartphone running the EcoStruxure Power Device app.

  • The smartphone must support Android 4.4 or iOS 9 or above, and be compatible with Bluetooth Low Energy wireless technology.

  • You must have access to the MicroLogic X control unit, and be physically within an open field range of 20 to 30 meters (22 to 32 yards) (within 10 meters (11 yards) for optimized connection) for the duration of the connection.

Enabling and Disabling Bluetooth Low Energy Communication

By default, Bluetooth Low Energy communication is disabled.

Bluetooth Low Energy communication can be enabled or disabled as follows:

  • On the MicroLogic X display screen, at Home > Configuration > Communication > Bluetooth, set Bluetooth to ON or OFF.

  • With EcoStruxure Power Commission software, at Home > Configuration > Communication > Bluetooth, set Bluetooth activation to ON or OFF.

The Bluetooth Low Energy communication status (enabled or disabled) can be displayed as follows:

  • On the MicroLogic X display screen, at Home > Communication > Bluetooth

  • With EcoStruxure Power Commission software

  • On a remote controller using the communication network

Predefined Events

Enabling Bluetooth communication generates the following event:

Code

Event

History

Severity

0x1429 (5161)

Bluetooth communication enabled

Communication

Low

0x1427 (5159)

Connection on Bluetooth port

Communication

Low

Setting the Bluetooth Disconnection Timer

When Bluetooth communication is activated using the activation pushbutton on the MicroLogic X control unit, there is a timer on the connection with a smartphone that ends the communication after a period of idle time. By default, this automatic disconnection timer is set to 15 minutes.

The setting for the Bluetooth disconnection timer can be changed as follows:

  • On the MicroLogic X display screen, at Home > Configuration > Communication > Bluetooth, set Bluetooth to ON, and then set the BLE timer (min) value.

  • With EcoStruxure Power Commission software, at Home > Configuration > Communication > Bluetooth, set Bluetooth time out delay (min) to the appropriate value.

You can set the value from 5 to 60 minutes (default = 15 minutes) in increments of 1.

Establishing a Bluetooth Low Energy Connection

Follow the steps below to establish a Bluetooth Low Energy connection from your smartphone to the MicroLogic X control unit.

Step

Action

1

Start EcoStruxure Power Device app on your smartphone.

2

Select to connect to device through Bluetooth.

3

On the MicroLogic X control unit, press the Bluetooth activation pushbutton.

The Bluetooth LED lights up. If it does not, you must enable the Bluetooth communication feature first.

On your smartphone, the EcoStruxure Power Device app starts scanning and displays a list of Bluetooth devices in the neighborhood. MicroLogic X control units are identified by their ID number.

4

Select the MicroLogic X control unit to which you want to connect.

A 6-digit pairing code is displayed on the MicroLogic X display screen.

5

Enter the pairing code in EcoStruxure Power Device app within 30 seconds.

  • If the pairing code is incorrect, or if more than 30 seconds have elapsed, Bluetooth communication is deactivated (the LED turns off), and you must start the connection procedure again at Step 3.

  • If the connection is established, the Bluetooth LED starts blinking.

6

To end the connection, you can either:

  • Press the Bluetooth pushbutton on the MicroLogic X control unit.

  • Disconnect from EcoStruxure Power Device app.

While your smartphone remains within the communication range (an open field range of 20 to 30 meters (22 to 32 yards) from the MicroLogic X control unit), the Bluetooth Low Energy connection remains active and the information displayed is refreshed.

NOTE: Each connection is unique, you cannot save the connection parameters for your next Bluetooth Low Energy connection.

Bluetooth LED

The Bluetooth LED on the front face of the MicroLogic X control unit can be:

  • ON: A Bluetooth connection procedure is in progress.

  • OFF: Bluetooth is not activated or disabled.

  • Blinking: A Bluetooth connection is established and active.

NOTE: The Bluetooth LED does not indicate whether the Bluetooth Low Energy communication feature is enabled or disabled in the MicroLogic X control unit. When this feature is disabled, the LED does not light up when you press the Bluetooth activation button.

Troubleshooting Bluetooth Low Energy Communication Issues

The following table lists common problems when establishing a Bluetooth connection to the MicroLogic X control unit.

Problem description

Probable causes

Solutions

The Bluetooth LED does not light up when you press the Bluetooth activation pushbutton on the MicroLogic X control unit.

The Bluetooth function is not enabled in the MicroLogic X control unit.

Enable Bluetooth communication in the MicroLogic X control unit.

The MicroLogic X control unit is not powered.

Check the power supply of the MicroLogic X control unit.

The Bluetooth connection was established but the signal is lost.

The smartphone has been moved out of range.

Place the smartphone within the range for Bluetooth and establish a new connection.

The Bluetooth LED is blinking on the control unit but you cannot see its ID number in the list of devices available.

A smartphone is already connected to the MicroLogic X control unit.

Check whether another smartphone within range is also connected to the control unit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.