PKR8059501

Maintenance

Read and understand the following precautions before performing any maintenance. See Requirements for Installation, Operation, and Maintenance for additional information.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, NOM-029-STPS-2011, or CSA Z462 or local equivalent.
  • Only qualified personnel familiar with medium voltage equipment are to perform work described in this set of instructions. Workers must understand the hazards involved in working with or near medium voltage circuits.
  • Perform such work only after reading and understanding all of the instructions contained in this bulletin.
  • Turn off all power supplying this equipment before working on or inside equipment.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Inspection and maintenance should only be performed with the primary source(s) of power disconnected and locked open. Be sure there is no back-feed through any feeder circuit.
  • Before performing visual inspections, tests, or maintenance on the equipment, disconnect all sources of electric power. Assume that all circuits are live until they have been completely de-energized, tested, grounded, and tagged. Pay particular attention to the design of the power system. Consider all sources of power, including the possibility of backfeeding. More than one disconnector switch may be required to de-energize the equipment before servicing.
  • Disconnect, de-energize, lockout and properly ground circuit(s) before working on the equipment.
  • Operate the switches with dry hands to prevent an electrical hazard.
  • Do not open the front cover while the power is on or the starter is running.
  • Disconnect the equipment and enable a lockout command prior to performing maintenance on the equipment.
  • Ensure that any stored energy in the capacitors has dissipated before energizing or de-energizing the equipment.
  • Carefully inspect your work area and remove any tools and objects left inside the equipment.
  • Replace all devices, doors, and covers before turning on power to 
this equipment.
  • All instructions in this manual are written with the assumption that the customer has taken these measures before performing maintenance 
or testing.
Failure to follow these instructions will result in death or serious injury.

Regular Inspections

Regular Inspections Frequency

Environmental Conditions

Inspection Frequency

Normal conditions, such as:

  • Ambient air temperature is between 14°F (-10°C) and 104°F (40°C)

  • Relative humidity is non-condensing and below 75%

  • Altitude is less than 3300 ft (1000 m)

  • Effect of solar radiation is not significant

  • No excessive pollutants or dirt in the immediate environment

  • No excessive vibrations

  • No electrical overloads

  • Usage of mechanical components such as disconnect switches less than 500 operations per year

Every year

Harsh conditions, such as:

  • Ambient air temperature is less than 14°F (-10°C) or greater than 104°F (40°C)

  • Relative humidity is above 75% and non-condensing

  • Altitude is greater than 3300 ft (1000 m)

  • Effect of solar radiation is significant

  • Excessive pollutants or dirt in the immediate environment

  • Excessive vibrations

  • Electrical overloads

  • Usage of mechanical components such as disconnect switches exceeding 500 operations per year

Every three months

NOTE: If issues are found during the inspection that require adjustment or repair, contact your local Schneider Electric field sales representative.

Cleaning the Switch Components

All switch components, including insulators and blade assemblies must be cleaned as follows:

  • Every year or after 1000 operations

  • Wipe the dust from the components with a clean dry cloth. After cleaning, apply a light coat of non-corrosive high-temperature grease that will not harden upon exposure to air (SHC-32 Mobiltemp or equivalent) to all contact surfaces.

Contact Inspection

Check the blades and ensure that they are making good contact.

  • Take a contact resistance measurement between (1) the jaw and spade terminal and (2) the hinge spade terminals. It should read between 38 to 100 micro-ohms for a new, unused switch.

  • Ensure that the blades can be "opened" from the jaw casting with a pulling force of 30–36 pounds measured at a point between the main blades, just below the jaw contact.

  • Wipe and clean the contacts, especially if the switch has not been in operation for a while. Open and close the switch several times in succession to do so.


CAUTION
Switch blade contact Damage
Do not clean the blades with abrasive materials or abrasive cleaners.
Failure to follow these instructions can result in injury or equipment damage.

Insulators

Keep all insulator surfaces clean, particularly when the switches are in harsh environmental conditions. Clean the insulators with a clean lint-free cloth dampened with either denatured alcohol or isopropyl alcohol.

Carefully inspect all insulators for signs of carbon tracking. Focus on areas where the conductor passes through an insulator or are near a barrier. Examine the surface for cracks or discoloration. Contact your Schneider Electric field sales representative if any of these conditions exist.

Bus and Conductor (Switch Blade)

Inspect the bus and connections for evidence of overheating or damage.

  • Using an appropriate insulation tester or Megger, measure and record the resistance to ground, and the resistance between phases of the bus and connections insulation.

  • Measure and record the ambient temperature and humidity.

Analyze these readings over consecutive periods to identify trends indicating insulation degradation.

Operating Shaft

The operating shaft connects the stored energy mechanism to the switch operating arm. Lightly coat the shaft bearings, door interlocks, and door latch surfaces with lubricant (white lithium grease).

Push Rods

Each main blade in the switch is connected to the main operating shaft by an insulating pushrod. Check the pushrods for signs of damage to either end each time a normal maintenance inspection is performed.

Stored Energy Mechanism

The stored energy mechanism consists of a housing with a one-piece crank sprocket assembly supported by bearings and a spring assembly. The sprocket assembly is chain-driven using the operating handle on the front of the enclosure. As the handle is moved upward, the spring assembly is charged. As the crank sprocket assembly passes over the center position, the spring takes control and drives the switch to the closed position.

The moving parts are the front and rear latches, which are spring-operated, and the two shaft bearings. Check the moving parts after approximately 100 operations to make sure the latches rotate freely up and down using finger pressure on the rollers. Check for loose bearing bolts.

Lubrication

Mechanical (non-electrical contacts): Clean and lubricate the bearing points and sliding surfaces at regular intervals with a thin film of white lithium grease. Before lubrication, remove any hardened grease and dirt from the latch and bearing surfaces with a clean, dry lint-free cloth.

Disconnector switch contacts: Clean and grease the contact surface of the movable blades and the stationary contact surfaces with SCH-32 Mobiltemp, or equivalent.

High Potential Tests

Perform a one minute high potential test on the primary circuit, busing and interrupter switch, at a field test value of either 14 kV AC or 20 kV DC.

Maintenance Checklist

The following tables list the inspection checks that are necessary to maintain and to verify that the equipment remains operational.

Cable and Bus Checklist

  Inspect bolts on bus connections for tightness
  Check clearance phase-to-phase and phase-to-ground of cable and bus.
  Check the bus and cable supports to verify they are adequate.
  Inspect the cables for insulation damage and broken conductor strands near the cable lug.
  Inspect the cable termination in the cable lugs for tightness.
  Inspect the placement of phase markings.
  Check the plating on busbars.
  Inspect the taped joints for tightness (when applicable).
  Check the connections on the lugs.
  Inspect the taped joints for coverage of insulating varnish and heating.

Key Interlocks Checklist

  Check the door block for lubrication.
  Check the key interlock system for appropriate sequence and operation.
  Verify that the interlock is free from binding.
  Check to verify the weather cap fits securely (outdoor only).
  Ensure that the key nameplate matches the key number.
  Check to verify that the handle stops on casting do not interfere with the interlock mechanism.
  Remove all spare keys.

Fuse Accessories Checklist

  Check contact of fuses mounted in the fuse clip.
  Inspect the unit for spare fuse holder or mounting.
  Check the alignment of fuses with the fuse clips.

Unit General Misc. Checklist

  Inspect the phase barriers for proper mounting.
  Check the unit for nomenclature and manufacturer's nameplates.
  Inspect the paint coverage of unit.
  Inspect the door handles, locking bars and mechanism and lubricate.
  Inspect for damaged, bent, or twisted doors.
  Check the unit for proper device markings.
  Inspect the unit for gasketed joints (outdoor only).
  Check the unit for water tightness, dirt, moisture, and rust.
  Inspect the unit for door stop alignment (when applicable).
  Inspect the unit doors for adequate opening.
  Check the louvers (if applicable) for proper backup and clean filters.
  Seal all non-ventilation openings to help prevent moisture, vermin, rodents, snakes, etc. from entering the equipment.
  Check the insulator for heat.
  Check and torque all bolts.
  Check the heaters, thermostats, and other environmental controls.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.