Routine End-User Preventive Maintenance Program

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Definition

The Routine end-user preventive maintenance program can be carried out by:

  • Trained and qualified end-user personnel.

  • Trained and qualified maintenance services provider personnel.

  • Schneider Electric Services representatives.

The Routine end-user preventive maintenance program comprises:

  • Limited visual inspection.

  • Function checks.

  • Replacement by standard exchange of certain assemblies.

The Routine end-user preventive maintenance program must be performed every year in the case of normal operating conditions. Refer to the recommended frequency for the Routine end-user maintenance program for other cases.

Procedures

The Routine end-user procedures are described in detail in MasterPacT MTZ with MicroLogic X Control Units - End-User Maintenance Procedures for IEC DevicesMasterPacT NT/NW - Routine and Intermediate End-User Maintenance Procedures for IEC Devices.

The Routine end-user procedures are described in detail in DOCA0306•• MasterPacT MTZ IEC Circuit Breakers with MicroLogic Active Control Unit - End-User Maintenance Procedures .

Part

Procedure title

Procedure name

Device

Check the general condition of the device

Device NII_Z_1

Mechanism

Operate the device manually and electrically

Mechanism NII_Z_1

Charge the device electrically with MCH gear motor

Mechanism NII_Z_2

Check the complete closing of device poles

Mechanism NII_Z_3

Auxiliaries

Check auxiliary wiring and insulation

Auxiliaries NII_Z_1

Control unit

Check device tripping and operation of SDE fault-trip indication contacts

Control Unit NII_Z_1

Check ground-fault (MicroLogic 6.0 X) or earth-leakage (MicroLogic 7.0 X) protection function

Control Unit NII_Z_2

Check operation of Energy Reduction Maintenance Settings (ERMS)

Control Unit NII_Z_3

Device locking

Operate device keylocks

Device Locking NII_Z_1

Operate device padlocks

Device Locking NII_Z_2

Chassis

Check device racking operation

Chassis NII_Z_1

Check IBPO racking interlock between racking handle and opening pushbutton (MasterPacT MTZ2/MTZ3)

Chassis NII_Z_2

Check EIFE chassis position limit switches

Chassis NII_Z_3

Chassis locking

Operate chassis keylocking system

Chassis Locking NII_Z_1

Operate chassis padlocking system

Chassis Locking NII_Z_2

Mechanical interlocking

Operate interlocking systems

Mechanical Interlocking NII_Z_1

Part

Procedure title

Procedure name

Device

Check the general condition of the device

Device NII_1_1

Mechanism

Operate the device manually and electrically

Mechanism NII_1_1

Charge the device electrically with MCH gear motor

Mechanism NII_1_2

Check the complete closing of device poles

Mechanism NII_1_3

Auxiliaries

Check auxiliary wiring and insulation

Auxiliaries NII_1_1

Control unit

Check device tripping and operation of SDE fault-trip indication contacts

Control Unit NII_1_1

Check ground-fault or earth-leakage protection function

Control Unit NII_1_2

Device locking

Operate device keylocks

Device Locking NII_1_1

Operate device padlocks

Device Locking NII_1_2

Chassis

Check device racking operation

Chassis NII_1_1

Check IBPO racking interlock between racking handle and opening pushbutton (MasterPact NW)

Chassis NII_1_2

Chassis locking

Operate chassis keylocking system

Chassis Locking NII_1_1

Operate chassis padlocking system

Chassis Locking NII_1_2

Mechanical interlocking

Operate chassis interlocking systems

Mechanical Interlocking NII_1_1

Part

Procedure title

Procedure name

Device

Check the general condition of the device

Device NII_ZA_1

Mechanism

Operate the device manually and electrically

Mechanism NII_ZA_1

Charge the device electrically with MCH gear motor

Mechanism NII_ZA_2

Check the complete closing of device poles

Mechanism NII_ZA_3

Auxiliaries

Check auxiliary wiring and insulation

Auxiliaries NII_ZA_1

Control unit

Check device tripping and operation of SDE fault-trip indication contacts

Control Unit NII_ZA_1

Check ground-fault protection function (MicroLogic Active 6.0)

Control Unit NII_ZA_2

Check operation of Energy Reduction Maintenance Settings (ERMS)

Control Unit NII_ZA_3

Device locking

Operate device keylocks

Device Locking NII_ZA_1

Operate device padlocks

Device Locking NII_ZA_2

Chassis

Check device racking operation

Chassis NII_ZA_1

Check IBPO racking interlock between racking handle and opening pushbutton (MasterPacT MTZ2/MTZ3)

Chassis NII_ZA_2

Chassis locking

Operate chassis keylocking system

Chassis Locking NII_ZA_1

Operate chassis padlocking system

Chassis Locking NII_ZA_2

Mechanical interlocking

Operate interlocking systems

Mechanical Interlocking NII_ZA_1

Tools

Performing the procedures of the maintenance program requires the following:

Time Required

The average total time required for experienced, trained, and qualified personnel to perform this maintenance program is as follows:

  • 15 minutes for a fixed device with all accessories installed

  • 20 minutes for a drawout device with all accessories installed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?