How to Maintain the Case

@TW: profiled topic used in Maintenance Guides: DOCA0305 (MTZ with Mic Act), DOCA0099 (MTZ with Mic X), LVPED508016 (NT/NW)

Functions

The case of the device:

  • Insulates the main contacts

  • Helps to protect the user against arcing effects

  • Provides a support for:

    • Mechanism

    • Control unit

    • Auxiliaries

    • Power connection

  • Withstands the thermal and electrodynamic stresses generated during short-circuits

Degradation Factors

The factors which can cause degradation of the case are the following:

  • Dusty or dirty environment

  • Humidity

  • High ambient temperature

  • Shocks

  • Stresses due to high short-circuit currents

Potential Hazards

Performing regular maintenance on the case can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Arc flash

Death or serious injury

Insulation resistance of the case too low and impulse voltage

Electric shock

Disruptive discharge

Degradation of the breaking unit

High short-circuit current

Degradation of the breaking unit

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the case of the device.

Maintenance program

Preventive action

Procedure

Routine end-user preventive maintenance

Check the general condition of the device.

Device NII_Z_1

Device NII_1_1

Device NII_ZA_1

Manufacturer preventive maintenance

Measure the insulation resistance.

Contact your Schneider Electric Services representative.

For more information, refer to Preventive Maintenance Programs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?