How to Maintain the Communication System

Functions

The communication system allows data transmission between the device and the remote controller. It can be used to remotely operate (open/close) the device.

Maintenance, production, management, and other departments can use this function to manage energy and assets, and monitor the quality of the electrical network.

In MasterPacT MTZMasterPacT NT/NW circuit breakers, the device data can be accessed by using the ULP port module connected to aan IFE or IFM communication interface and an appropriate software tool such as EcoStruxure Power Commission software.

MasterPacT MTZMasterPacT NT/NW devices with communication interface:

Degradation Factors

The factors which can cause degradation of the communication system are the following:

  • Vibration

  • Electro-magnetic field disturbances

  • Equipment and software breakdown

  • Modification of communication system architecture

Potential Hazards

Performing regular maintenance on the communication system can help to avoid the potential hazards and consequences listed in the following table.

Hazard

Consequence

Personal injury

Equipment damage

Incorrect or no operation (critical to safety) as a result of misleading information

Death or serious injury

Communication loss

Inappropriate functioning of devices, communication interfaces or modules on communication network

Incorrect decision taken as a result of misleading information (status, metering, health)

Inappropriate functioning of devices, communication interfaces or modules on communication network

Incorrect system management leading to financial losses

Inappropriate functioning of devices, communication interfaces or modules on communication network

Preventive Action

The following table lists the preventive maintenance procedures to be performed to maintain the communication system.

Maintenance program

Preventive action

Procedure

Manufacturer preventive maintenance

Check data transmission over the IFE Ethernet interface or EIFE embedded Ethernet interface.

Check data transmission via communication bus

Contact your Schneider Electric Services representative.

For more information, refer to Preventive Maintenance Programs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?