Influence of Salt Environment on Aging
Salt Environment
Influence |
Appearance |
Consequences |
---|---|---|
Corrosion of metal parts |
Appearance of:
|
|
Possibility of salt deposits on electronic circuits when thick salt mists occur. |
Appearance of salt bridges on electronic boards |
Potential failure of electronic systems due to short-circuiting of circuits, particularly non-varnished circuits. |
Possibility of conducting salt deposits on the device when thick salt mists occur. |
White deposit |
Deterioration of device dielectric withstand resulting in possibility of phase-to-frame short-circuit and a phase-to-phase short-circuit if an overload occurs. |
Recommendations
The maintenance and installation recommendations according to the salt environment are defined in the following table:
Thresholds |
Description |
Maintenance recommendations |
Installation recommendations |
---|---|---|---|
No salt mist |
No influence |
Implement the Intermediate program. |
No particular recommendation |
Moderate salt mist < 10 km (6.21 miles) from coast |
Moderate aging of switchgear |
Carry out more frequent periodic checks. |
No particular recommendation |
Significant salt mist < 1 km (0.621 miles) from coast |
|
|
|