Section 16: NEMA and Definite Purpose Contactors and Starters
For voltage codes used with control transformers, see Control Circuit Transformer Codes. Form S (separate control) is used when a separate source of power is available for the control (coil) voltage. Available at no charge. Dimensions: Open and NEMA 1Factory Modifications (Forms) Full Voltage
mounted upright on the vertical plane; the contactors will not operate properly when mounted in any other position. AC Reversing/Hoist Contactors—600 Vac Maximum No. ofPoles Horsepower Ratings PowerTerminals With Jumper straps connect the line side power terminals of the same phase between the