63249-403-200

Setting the Address

Each secondary address selector accessory must have a unique address. To assign addresses to secondary panels, follow these steps:

  1. Locate the address setting dial on the secondary address selector (see Figure 2).

    Rotary Dial on Secondary Address Selector Accessory

  2. Use a screwdriver with a 1/8 in. flat head to turn the dial so the arrow on the dial points to the desired address.

  3. Continue setting any additional secondary panelboards in this same manner, making sure each panelboard has a unique address.

    NOTE: If two or more secondary panels share the same address, they will not operate as intended.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?