63249-420-374

Safety Information

Read these instructions carefully and examine the equipment to become familiar with the device before attempting to install, operate, service, or maintain it. The following special messages may appear throughout this user guide or on the equipment to warn of hazards or to call attention to information that clarifies or simplifies a procedure.

The addition of either symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

 

This is the safety alert symbol. It is used to alert you to personal injury hazards. Obey all safety messages that follow this symbol to avoid possible injury or death.


NOTE: Provides additional information to clarify or simplify a procedure.

Please Note

Electrical equipment should be installed, operated, serviced, and maintained only by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.

Electrical equipment should be transported, stored, installed, and operated only in the environment for which it is designed.

FCC Class B

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

  • Reorient or relocate the receiving antenna.

  • Increase the separation between the equipment and receiver.

  • Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.

  • Consult the dealer or an experienced radio/TV technician for help.

The user is cautioned that any changes or modifications to this device that are not expressly approved by Schneider Electric could void the user’s authority to operate this equipment.

This digital apparatus complies with CAN ICES-3 (B) /NMB-3(B).

About This Bulletin

This bulletin explains how to install the Powerlink NF3500G4 Controller, which is used to control the operation of a Powerlink G4 system. The controller uses remotely operated circuit breakers to control up to 336 remotely operated branch circuits. Control signals originate externally from dry-contact inputs, from the internal time scheduler, or from commands received via the communications network. Typical control devices include low voltage pushbutton wall switches, occupancy sensors, photocell controllers, and security and building management systems.

Refer to “Powerlink NF3500G4 Controller User’s Guide 63249-420-409” for more information about:

  • Configuration using the controller’s LCD screen navigation

  • Installing using LCS software to a PC for configuration

  • The current version firmware

Before You Begin

Before installing the NF3500G4, inspect it carefully. Verify the catalog number on the box label.

Components

Part Number Description Quantity

NF3500G4

Powerlink Controller 1
  Class 2 barrier 1
 

Connector hardware kit

  • 9 three-terminal connectors

  • 1 four-terminal connector

  • 2 two-terminal connectors

1
  Miscellaneous hardware kit (screwdriver, tie wrap, panelboard reference label) 1
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.