63249-420-374

Connecting an External Device to Multiple Controllers

An external device may be wired to multiple controllers. It is recommended that the source voltage be provided to the external device by one controller. The input signal from the external device and the circuit common terminal on the common ground connector are connected to the other controllers.

Connecting External Devices to Multiple Controllers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.