63249-420-374

Front Panel Overview

Components of the Controller shows the parts of the controller’s front panel. A brief description of each part can be found in Features of the Controller Front Panel.

Components of the Controller

Features of the Controller Front Panel

Component Description
A LCD Screen The LCD screen displays the information to set up and operate programs for the controller.
B Wiring compartment The wiring compartment cover protects the input and communications port terminals located in the Class 2 wiring compartment. To remove and install the compartment cover, see Installing the Class 2 Barrier. See Controller Class 2 Communications Terminals Detail for an overview of the wiring compartment terminals.
C Temporary RJ45 communications port The temporary RJ45 communications port is used for a temporary connection to a PC.
D Plus key/Enter key The Plus key/Enter key scrolls through the choices for an option on the LCD screen and selects items on the screen. If the cursor is on a numeric field, the Plus key/Enter key increases the value.
E Minus key The Minus key scrolls through the choices for an option on the LCD screen and de-selects items on the screen. If the cursor is on a numeric field, the Minus key decreases the value.
F Next key The Next key moves the cursor to the next option on the LCD screen.
G Back key The Back key moves the cursor to the previous option on the LCD screen.
H Reset button The Reset button reboots the controller.
I Power/Communications supply connection (to the power supply) Connects to the power supply.

Controller Wiring Compartment Components



Controller Class 2 Communications Terminals Detail

Wiring Compartment Components

Component Description
A RJ45 Ethernet Ports (2) Use this port to connect the controller to a network.
B RS232 Communications Use these terminals to connect to external RS232 communication.
C RS485 Communications Terminals Use these terminals to connect to external RS485 communication.
D Input Terminals (See Wiring Compartment Components.) (1–16) Use these terminals to connect to an external dry-contact switching device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.