DUG_Motion_Sensor_PDL–00

Installing the device

Refer to the installation instruction supplied with this product.
See Wiser Motion Sensor.
NOTICE
RISK OF DAMAGE TO DEVICE
  • Always operate the product in compliance with the specified technical data.
  • Do not install the sensor in a place with strong sunlight or wind (for example, close to ventilation).
  • Temperatures greater than 32 °C degrade the sensor's ability to measure sensitivity, detection range, and angle.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?