LED Indications
Initial Stage
Action |
LED Indication |
Status |
Green LED blinks 7 times (1 Hz) |
After the sensor is powered On for the first time or after the batteries were replaced. |
If not paired yet
If already paired
Reset - After pressing the function key 3 times within 0.5 seconds and then hold for 10 seconds
Action |
LED Indication |
The red LED blinks for 10 seconds, remains on for 3 seconds, and then turns off. The sensor then restarts and blinks green for a few seconds. |
Battery level
LED Indication |
Status |
LED blinks amber once per minute. |
The battery is low (< 10%), replace the battery. NOTE: A notification pop-up
will appear on the app.
|