DUG_Motion_Sensor_PDL–00

Lux Setting

Using the Wiser app, you can define the threshold value for lux ranges (such as very dark, dark, bright, very bright) of the environment. This will prevent the false alarm caused by changes in the light intensity.
To set the lux range value:
  1. On the Home page, tap All devices > Motion Sensor.
  2. On the device control panel page, tap Settings.
  3. Tap any of the following Lux ranges and drag the slider bar to define its threshold value and tap Save:
    • Very dark level - Lux value ranges from 1 lux to 100 lux
    • Dark level - Lux level ranges from 6 lux to 300 lux
    • Bright level - Lux level ranges from 101 lux to 2000 lux
    NOTE: The Current Lux Value is the current light level present in the environment, which the sensor can measure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?