DUG_Smoke alarm DC_PDL-00

Checking the device history

Using the Wiser app, you can monitor the smoke detection by accessing the device history.
To see the device history:
  1. On the Home page, tap All devices > Smoke Alarm.
  2. On the device control panel page, tap History.
  3. In the History page, you can see the date, time, and type of alarm detected.

    NOTE: The history supports record checking for 7 days maximum.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?