DUG_Smoke alarm DC_PDL-00

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
To pair the device:
  1. Locate the power switch on the rear side of the device. Use a screwdriver to turn the power switch to ON position.
  2. On the Home page, tap +.
  3. Tap Auto scan and than tap Confirm.
  4. If you have multiple hubs, do Step 4 or proceed to Step 5.
  5. Tap Select hub and select the Wiser hub from the slide-up menu.
  6. Press the Set/Reset button 3 times within 2 s.
    NOTE:
    • The LED blinks yellow.

    • Wait for a few seconds until the device search is complete.

    TIP: If you want to pair multiple devices at once, perform step 5 on each device and wait for a few seconds for them to be detected.
  7. Select Smoke Alarm and tap Next (A).

  8. Once the device is added successfully, tap Done.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?