DUG_Smoke alarm DC_PDL-00

About the device

The Wiser Smoke Alarm – Battery (device) uses a photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat caused by rapid increase in temperature. When connected to the Wiser system the device sends the notifications via the Wiser app.

Operating elements

  1. Status LED (Amber, Green and Red LED)

  2. Standby LED (Red LED)

  3. Test/Hush button

  4. Power switch

  5. Setup/Reset button

Installation location

  • Smoke Alarm can be installed on a flat/inclined ceiling, or on the wall.

  • Do not install smoke alarms near windows, doors, or ducts.

  • Avoid paint, stickers, or other decorations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?