DUG_Temperature and Humidity Sensor_PDL-00

Installing the device

Refer to the installation instruction supplied with this product.

See Wiser Temperature Humidity Sensor.

NOTICE
EQUIPMENT DAMAGE
Do not install the sensor in a place where there is strong sunlight or wind (for example, close to the ventilation).
Failure to follow these instructions can result in equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?