DUG_Temperature and Humidity Sensor_PDL-00

LED indications

Initial Stage

Action

LED Indication

Status

Green LED blinks 7 times (1 Hz)

→ (7x)

After the sensor is powered On for the first time or after the batteries were replaced.

If not paired yet

Action

LED Indication

Status

Amber LED blinks (1 Hz)

→ (2 min) → (3 sec)

Indicates the pairing mode after function key is pressed 3 times within 1 second. If pairing is not successful, the amber LED is On for 3 seconds and then turns Off.

Green LED is On for 3 seconds

→ (3 sec)

Pairing was successful.

If already paired

Action

LED Indication

Status

Green LED blinks 5 times (1 Hz)

→ (5x)

The sensor is paired and connected.

An amber LED blinks for three seconds (4 Hz)

→ (3 sec)

The sensor is paired, but disconnected.

Reset - After pressing the function key 3 times within 0.5 seconds and then hold for 10 seconds

Action

LED Indication

The red LED blinks for 10 seconds, remains on for 3 seconds, and then turns off. The sensor then restarts and blinks green for a few seconds.

→ (10 sec) → (3 sec)

Battery level

LED Indication

Status

LED blinks amber once per minute.

The battery is low (< 10%), replace the battery.

NOTE: A notification pop-up will appear on the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?