DUG_IPC_Outdoor_PDL-02

Inserting a micro-SD card

The micro-SD card is inserted in the device to store the recording.
NOTE: The micro-SD card has to be inserted before you power On the device. If the device is already in On state, then switch Off the device to insert the micro-SD card.

Follow the steps to insert a micro-SD card:

  1. Remove the cover on the back of the camera.
  2. Insert a micro-SD card in the memory card slot.
  3. Close the cover.
    Once the micro-SD card is inserted, you can configure the playback settings.
    NOTE: A maximum of 128 GB SDHC and SDXC micro-SD cards with FAT32 format are supported.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?