DUG_IPC_Outdoor_PDL-02

Detection alarm setting

The motion detection function enables the IP camera to detect motion in the surveillance area and display notifications in the Wiser app.

Follow the steps to enable the motion detection:

  1. On the Home page, tap All devices > IP Camera Outdoor.

  2. Tap and tap Settings > Motion Detection.

  3. Tap the toggle switch (A) to turn On the Motion Detection Alerts.

TIP: Alternatively, you can tap the icon on the control panel.

Alarm sensitivity level

Using the Wiser app, you can adjust the sensitivity level of your motion detector.

Tap Alarm sensitivity level (B) and select any one of the following levels:

Low

Medium

High

NOTE: The high sensitivity level detects the slightest movement and triggers an alarm.

Activity area

Using the Wiser app. you can set the surveillance area for motion detection.

  1. Tap the toggle switch (C) to enable the Activity area.

  2. Tap Surveillance area settings (D) and drag/resize the red frame to set the surveillance area and tap Save.

NOTE:
  • The motion is detected only in the saved surveillance area.

  • The privacy zone detection area setting overrides the motion detection activity area setting. Therefore, even if the motion detection activity area is larger than the privacy zone detection area, the motion will only be detected within the privacy zone detection area.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?