Meter screen menus

All meter screens are grouped logically, according to their function. You can access any available meter screen by first selecting the Level 1 (top level) screen that contains it.

With the meter front panel, you can view parameter values; configure parameters; perform demand resets; perform LED checks; and view meter information. Each of these functions can be accomplished by pressing the Up, Down, and OK buttons on the front panel.

With the meter front panel, you can view parameter values; configure parameters; perform demand resets; perform LED checks; and view meter information. Each of these functions can be accomplished by pressing the Left, Up, Down, and OK buttons on the front panel.

With the meter front panel, you can view parameter values; configure parameters; perform energy resets (EM1250H and EM1220H); perform LED checks; and view meter information. Each of these functions can be accomplished by pressing the Left, Up, Down, and OK buttons on the front panel.

These button actions achieve different results according to the mode that the meter is in:

  • Display mode (default): view parameter measurements

  • Setup mode: configure a parameter

  • Diagnostics mode: verify that the front panel display LEDs are operational, and view meter information (e.g. meter model, firmware version, etc.)

  • Diagnostics mode: verify that the front panel display LCD is operational, and view meter information (e.g. meter model, firmware version, etc.)

  • Clear mode: reset measurements

  • Reset mode: reset measurements

  • Lock mode: lock or unlock a screen

This section describes front panel navigation within each mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?