Meter configuration

Meter configuration is performed through the display or through PowerLogic™ Siemens ION Setup .

ION Setup is a meter configuration tool that can be downloaded for free at www.se.com www.usa.siemens.com/pds .

See the EasyLogic PM2000 Series Power Meter in the ION Setup online help or in the ION Setup device configuration guide. To download a copy, go to www.se.com www.usa.siemens.com/pds and search for ION Setup device configuration guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?