Power quality

The meter provides complete harmonic distortion measurement, recording, and real-time reporting, up to the 15th harmonic for PM2120 and up to 31st harmonic for PM2130 for all voltage and current inputs.

The following power quality measurements are available:

  • PM2120: Individual odd harmonics up to 15th order (Voltage and current, per phase)

  • PM2130: Individual odd harmonics up to 31st order (Voltage and current, per phase)

  • Total harmonic distortion (THD%) for current and voltage (displays line-to-line or line-to-neutral, based on selected system configuration)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?