Meter Features
-
LED display screen: Intuitive self-guided navigation using three buttons LED display, with three lines of concurrent values. Two columns of LEDs given on the either side of the meter’s front panel indicate the parameter name being displayed.
-
Energy accounting and balancing
-
Measurement of both True PF and Displacement PF
-
Active, reactive, and apparent energy readings
-
Min/Max values of instantaneous parameters with timestamp.
-
Cybersecurity: The meter supports the disabling of RS-485 port through front panel keys to prevent unauthorized access. Toggle the RTU devices in case of limited availability of nodes in software system.
-
Suppression current: The meter can be configured to disregard the measurement of induced / auxiliary load current in the circuit (can be set from 5 to 99 mA).
You can use the meter as a stand-alone device, but its extensive capabilities are fully realized when used as part of an energy management system.
For applications, feature details and the most current and complete specifications of the PM2100 meters, see the EasyLogic PM2000 series technical datasheet at www.se.comwww.usa.siemens.com/pds.