Current demand

The meter calculates current demand using the block interval, synchronized or thermal demand methods.

You can set the demand interval from 1 to 60 minutes in 1-minute increments (for example, 15 minutes).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.