Quadrant based VARh

NOTE: Applicable only for PM2220/PM2230 meter models
NOTE: Applicable only for PM2220R/PM2230R meter models

Quadrant based reactive energy values are available only on communication. These are not available on meter display. These reactive energies are for Q1, Q2, Q3, and Q4 quadrants.

On communication quadrant based reactive energies will be recorded as follows:

  • Q1 (00 to 90 Degree) = Q1 VARh , Del

  • Q2 (90 to 180 Degree) = Q2 VARh , Del

  • Q3 (180 to 270 degree) = Q3 VARh, Rec

  • Q4 (270 to 360 degree) = Q4 VARh , Rec

If energy is cleared, all quadrant based VARhs will be cleared.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.