Min/Max values

When the readings reach their lowest or highest value, the meter updates and saves these min/max (minimum and maximum) quantities in non-volatile memory.

The meter’s real-time readings are updated once every 50 cycles for 50 Hz systems, or once every 60 cycles for 60 Hz systems.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.